AXIS#.FIELDWEAKENING.CURRFILTERBW
Description
This keyword determines the bandwidth of the second order low-pass biquad filters that are applied on the q-axis and d-axis currents for noise reduction. These currents are used inside the field weakening algorithm for regulating the motor-voltage-vector-magnitude when operating above base speed. Lower bandwidths result in cleaner signals but can also create phase lag and lower the phase margin of the system. Depending on the required speed of the motion, they can be adjusted.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-06-00-000 |
|
General Information
Type |
Read/Write |
Units |
Hz |
Range |
0 to 5000 Hz |
Default Value |
1500 Hz |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.FIELDWEAKENING.CURRFILTERBW |
5019h |
01h |
Signed32 |
- |
- |
Read/Write |
No |
AXIS2.FIELDWEAKENING.CURRFILTERBW |
5119h |
01h |
Signed32 |
- |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
7301 |
1 |
7301 (0x1c85) |
AXIS1.FIELDWEAKENING.CURRFILTERBW |
Signed32 |
Read/Write |
Yes |
72837 |
2 |
7301 (0x1c85) |
AXIS2.FIELDWEAKENING.CURRFILTERBW |
Signed32 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.FIELDWEAKENING.CURRFILTERBW |
7301 |
Signed32 |
Read/Write |
- |